Other Parts Discussed in Thread: TLV320AIC3268, TLV320AIC3263, TLV320AIC3262, TLV320AIC3212
Hi,
I'm new to the TI MiniDSP solution and have a hopefully simple question.
Is it possible to program the MiniDSP to decode samples: split 32 bit samples to two 16 bit samples, and threat them as separate input streams (to be mixed together)?
Background infos:
- The input signal can be regarded to be I2S multi-channel TDM mode. It's possible to select one of the input streams by programming the data offset register to 0 or 16. But we like to use them both.
- In the solution linked here, the signal is connected to multiple I2S inputs, one with offset 0 and the other with 16. But the secondary I2S input of the TLV320AIC3254 cannot be active together with the primary one it seems. So we would have to upgrade the DSP to use this solution.
- Signals look as follows (the dual stream one):
Thanks for your support.