For the differential input stage 1, what is the minimal value of R2 (see page 11 of spec)?
The datasheet gives the range of 34−100 kΩ.
This implies that the minimum value is 34 ohms or it is 34K ohms
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For the differential input stage 1, what is the minimal value of R2 (see page 11 of spec)?
The datasheet gives the range of 34−100 kΩ.
This implies that the minimum value is 34 ohms or it is 34K ohms
Hi Al,
I believe it is 34kohms - 100kohms.
Regards,
Aaron Estrada
Thanks. I suspected it was 34K ohms but the datasheet was vague on the lower end resistance and required more clarification.