Hello team
I want to high power output 50W@THD3%;4ohm by TAS6424-Q1.
In this case, the supply voltage to PVDD is 22V. But, if 22V input to VBAT, TAS6424-Q1 is shutdown by the OverVoltage (OV).
**The Battery voltage is 24V system. 22V is made by Buck-Boost converter.
I'm thinking of making 12V from 22V, but the description below is in Section [10.3.9.2 Boosted Power-Supply Sequence ],
『In this case, the VBAT and PVDD inputs are not connected to the same supply.
When powering up, apply the VBAT supply first, the VDD supply second, and the PVDD supply last.
When powering down, remove the PVDD supply first, the VDD supply second, and the VBAT supply last.』
~Question~
What are the concerns when inputting in the order of PVDD -> VBAT -> VDD? What happens at the IC?
I am thinking of using PVDD -> VBAT -> VDD in the power-on sequence and VDD -> VBAT -> PVDD in the power-down sequence.