Hi Sir,
I have encountered several problems when designing with TS3A227 and ALC256 (Audio Codec), and the schematic diagram of TS3A227 is as follows:
My problems are as follows:
1) Did the DVT circuit can realized the control of the earphone function and the wire control function? Is there any problem with the line connection and need to be adjusted?
2) When the rear LINE IN or LINE OUT is inserted first, and then the front earphone is inserted, the front MIC can be recognized, but the MIC function does not work normally. we have found that TS3A227 has no signal sent to PORTB, and the other port functions are correctly identified and functioning normally.
3) Insert the 4-segment earphone on the front panel, the MIC wind function of the front panel earphone is abnormal.The voltage of the AR1058/AR1060 resistance terminal is measured to be 0V, while the normal recognition is about 2.28V.
Can u help to check if there is any problem with the circuit design and give some suggestions? If the entire circuit design was needed, I can send it to you offline.
Thanks,
Best Regards