Other Parts Discussed in Thread: PCM1808
Do you have relationship between analog input and Vcc of PCM1862 as PCM1808 ds shows as below?
Thanks, Ian.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ian,
The PCM186x family has an input attenuator on the front end allowing it to support a wider input range. The full scale range of the device should not change significantly between the 3.0V and 3.6V specified operating range. The inputs should still be limited as given in the abs max table though
Best,
Zak