Dear Sir, Madame,
In the Purepath SW I have modeled my speaker (configuration: passive radiator) by entering the T/S parameters, the enclosure parameters (inclusive passive radiator properties). For the SOA limits, I entered the peak excursion limits and thermal limits of the driver (I do not have the Smart amplifier learning board)
The Purpath Console SW calculates correctly the Speaker response (as compared to another simulation program), however, it seems that PurePath does not provide the excursion information.
In addition, when playing audio, there is no protection against over excursion of the speaker (severe clipping of the speaker).
The excursion of the speaker can only be reduced by entering an unrealistic small excursion value (more than a factor 5 smaller).
1. Why is the excursion not calculated for a speaker with a passive radiator? (it seems it works for closed speaker boxes and boxes with a vent)
2. If the program cannot calculate the excursion curves, can I apply these curves manually?
3. If item 2 is not possible how can I we get the speaker excursion protection work correct?
Thanks and best regards
Roel