Other Parts Discussed in Thread: PCM1754, PCM5102
Hello,
does it support 16-bit(not 24-bit) i2s?
i'm porting the pcm1754 to an embedded linux system.
and it is set to I2S 16bit mode but it didn't work.
but i connected to PCM5102 with the same wires(BCK,SCK,LRCK,DAT) and settings as PCM1754 and it works.
what makes these two chips different?
and i was able to get the following information from the Datasheet.
looking at the above data, i don't know if it supports 16bit i2s.
please teach me.
ps: looking at the datasheet, it seems that i2s mode doesn't supoort 256fs, is this also true?
thank you.