Other Parts Discussed in Thread: ADS127L01, TLV320ADC6140
Hi TI,
having just seen one of the new audio ADCs, TLV320ADC6120, I wonder why these ADCs are already sold / available but the power consumption specs in the datasheet are still "TBD"?
I mean, when the physical chip is available, why not just measure supply currents and put it in the datasheet?
Another general "audio" converter issue (sorry for the rant...):
Why do all the audio converter manufacturers build these "lousy" digital decimation filters into their audio ADCs?
With relatively low stop-band attenuation, and even worse, mostly a transition band that goes beyond 0.5 x fs.
There's more and more high frequency noise around these days, and why build 120dB+ SNR ADCs with stop-band attenuation of merely 70dB or 80dB?
I know TI can do better as shown with the ADS127L01 (my favorite ADC, also great DC specs, unfortunately only single channel, but used wherever possible in my designs) which has a really good filter reaching full stop-band attenuation (116dB) at half the sampling rate. With relatively low power consumption, too.
So please build better filters into your (otherwise very good) audio converters!