Per TLV320ADC3101 document, analog input voltage to AVSS shall be -0.3V ~ AVDD+0.3V
But from another case https://e2e.ti.com/support/audio/f/audio-forum/996671/tlv320adc3101-dc-voltage-measurement?tisearch=e2e-sitesearch&keymatch=tlv320adc3101%20DC#,
valid analog input voltage is 0.35V ~ 2.35V. How to understand this ? Can TLV320ADC3101 measure analog input voltage >2.35V or <0.35V ?
Probably can we use Analog PGA ( Page 1 / Register 59: Left Analog PGA Settings ) to adjust the input signal ? If yes, could you tell me the computational formula?
I did some test. The input DC voltage is 1277mv.
With 0dB gain, adc outputs 1277mv.
With 10dB gain, adc outputs 1120mv.
with 20dB gain, adc outputs 648mv
I am sorry I don't know the right formula for the actual test results
Thanks,
Burton