This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TLV320AIC3105EVM-K: Connect USB issue

Prodigy 20 points

Replies: 3

Views: 285

Part Number: TLV320AIC3105EVM-K

Hi,

I've got same problem as in the link below. The drivers are installed. All jumpers are set to default.

e2e.ti.com/.../707660

  • hi Adam,

    If you are using Windows vista, 7 or higher you will need to install the updated driver.  This is found on the EVM product folder under "software". The download is a folder named "slac521"  and it contains two files:

    1. USB-MODEVM_vista&7.inf

    2. USB-MODEVM_WDM.inf

    Instructions for installing these files:

    USB-MODEVM_vista&7.inf Installation:
     To apply the contents of this file to a system's settings, right-click
     this file and choose "Install". If the device was plugged in before this
     file is installed, the device will need to be removed from the "Unknown
     Devices" class in the Windows Device Manager.

    ---------------------------------------------------------------------------------------------

    USB-MODEVM_WDM.inf installation:

    To apply the contents of this file to a system's settings, copy this file
     to %SystemRoot%\inf and reboot the computer. If the device was
    installed before this file is copied, the device will need to be removed
    from the "Unknown Devices" class in the Windows Device Manager.

    best regards,

    -Steve wilson

  • In reply to Steve-Wilson:

    Hi Steve,

    I have already installed these drivers. The issue is still unsolved.

    I am using Windows 10 Enterprise.

    Best regards,

    Adam

  • In reply to Adam89:

    Adam,

    please take a look at this thread and follow along to see if this resolves your issue:
    e2e.ti.com/.../2345644

    best regards,
    -Steve Wilson

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.