This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TLV320AIC3101EVM-K: Can't corretly install the driver, I tested on win7 and xp

Intellectual 2490 points

Replies: 16

Views: 471

Part Number: TLV320AIC3101EVM-K

Hi,

I got this EVM recently, and plug in usb. But I can't correctly install the driver. the driver I used is from TI website as below. I tested on win7 and xp, but all failed【report that:"can't find the driver file"】. please suggest if something need to pay attention.  thanks.

Also tried the english path, result is the same. 

  • In reply to Steve-Wilson:

    Fully followed the instructions.  For sure,

    (1)I pulled out the USB cable as the first step,

    (2)next, short SDA (1)and SCL(3),

    (3)then power on  by plugging in USB, waited for 5s and above,

    (4)then, removed the jump between SDA and SCL

    (5) open the SW.

    I also do 5 then 4, That is to say, I opened the SW firstly,then remove the short. the result is same - "No DFU Device found"

  • In reply to Yue TANG:

    Yue,

    how are you shorting SDA and SCL?

    -steve
  • In reply to Steve-Wilson:

    Short SDA and SCL by connecting pins 1 and 3 of J6 on the USBMOD EVM. Just followed the instructions.

  • In reply to Steve-Wilson:

    I got another 3 three new boards. None of them can install the driver correctly. I also tried on several my colleage's laptops, all failed. headache!!!
  • In reply to Steve-Wilson:

    I also tried on an old laptop, but still failed. can you please direcly copy the driver from the "inf" folder and share to me? I'm very doubt the correction of the driver downloaded from the TI website.
  • In reply to Yue TANG:

    If you are the first time to use this EVM, install the driver as below attached. Also make sure the “SW2” in mother board is followed below description: 

    "SW-2 positions 1 through 7 should be set to ON, whereas SW-2.8 should be set to OFF"

    dfu_driver.7z

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.