This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 16
Views: 310
Part Number: TLV320AIC3101EVM-K
Hi,
I got this EVM recently, and plug in usb. But I can't correctly install the driver. the driver I used is from TI website as below. I tested on win7 and xp, but all failed【report that:"can't find the driver file"】. please suggest if something need to pay attention. thanks.
Also tried the english path, result is the same.
In reply to Steve-Wilson:
Hi Steve,
I fully followed below instructions on a winxp ,but always showed "unknown". I removed the "unkown device" in WDM. and tried below at least 3 times. each time, I plug in the USB, it also showed find a new device and try to install the driver, then fail. it is a bit frustrating. my customer also met the same problem.
can you double check if this driver is no problem? it is a bit urgent.
1. USB-MODEVM_vista&7.inf
2. USB-MODEVM_WDM.inf
Instructions for installing these files:
USB-MODEVM_vista&7.inf Installation: To apply the contents of this file to a system's settings, right-click this file and choose "Install". If the device was plugged in before this file is installed, the device will need to be removed from the "Unknown Devices" class in the Windows Device Manager.
---------------------------------------------------------------------------------------------
USB-MODEVM_WDM.inf installation:
To apply the contents of this file to a system's settings, copy this file to %SystemRoot%\inf and reboot the computer. If the device wasinstalled before this file is copied, the device will need to be removedfrom the "Unknown Devices" class in the Windows Device Manager.
In reply to Yue TANG:
No..still show as “unknown” in device management. I seriously doubt the driver ‘s correction. Both my customer and I failed to install the driver on all kinds of windows systems,even include the virtual machine . Would you please try the driver on a clear windows system which not install this driver before.if ok,please share the driver you correctly installed.thanks.
You can see this from the "USB-MODEVM_vista&7.inf"
[Version]Signature=$WINDOWS NT$Class=visaUsbDeviceClassGUID={A3330EDF-239D-4206-833B-1D58952613D5}Provider=%Vendor0%DriverVer=05/02/2012,1.0CatalogFile=USB-MODEVM_vista&7.cat