This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TAS5756MDCAEVM: Recently, a project used TI device TAS5756M, and a set of TAS5756MDCAEVM and control motherboard. During the test, the firmware of the test program MSP430F2132 was accidentally written and overwritten. Could you please provide the firmware

Prodigy 10 points

Replies: 2

Views: 139

Part Number: TAS5756MDCAEVM

Recently, a project used TI device TAS5756M, and a set of TAS5756MDCAEVM and control motherboard. During the test, the firmware of the test program MSP430F2132 was accidentally written and overwritten. Could you please provide the firmware of the test program MSP430F2132? thank you

  • hi,
    TAS5756 is combined with a PurePath™ Console Mother Board (PurePath-CMBEVM – must be ordered separately) and PurePath™ Console GUI (PurePathConsole – must be ordered separately) you have a complete audio evaluation system. we dont support MSP430 firmware code.
  • Hi Customer,

    Please go to MCU form to ask for the firmware of the test program. On audio amplifier's side, what we can provide is the registers configuration of TAS5756, which is is integrated in the programme you are secking. For this point, I think you can refer to Linda's suggestion to ask for a complete audio evalution system.
    But if you are firmware engineer, please go to MCU forum to ask for the code.

    Regards,
    Alix Wan.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.