All;
I have an application where I would like to use a pair of DRV601buffer amps to drive 4 line level audio outputs. Because of space constraints we would like to
be able to re-task two of the connectors to inputs under software control. The question is as the DRV601 has shutdown inputs for each of the outputs what
do I "see" when looking back into the outputs of the DRV601 when the shutdowns are asserted? Do they go to a high impedance state? Or will I need to isolate
them with an external switch to keep from loading an external signal trying to use the connector as an input?
Thanks... Don C.