This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

micro smd audio amp identification



Hi,

I have a number of IC's in small portable amplifiers that are faulty but I'm having trouble with identification of the device type.

They are micro smd 9 bump devices and I suspect they are class D 2w single channel audio amps.

The type markings appear to be:-

95W 17S

      BP 27

Although the top line does vary the BP 27 is consistent. Due to the size of these devices it's difficult to see the markings clearly. I have checked through the data sheets for all devices of this type and can't find anything that would match these codes.

Could you possibly tell me if it is a TI device and if so what LMxxxx it might be?

Many thanks

Bob