Dear Sirs,
we are running the PCM2903B AUDIO CODEC chip under WINDOWS XP witout any problems.
Under WINDOWS 7 we now have the problem that ADC input chanels can not be used for recording because the input level can not be controlled.
Is there any solutions for this problem or can you suggest another chip with the same function running under WINDOWS 7?
Kind regards
--
Andreas Richter
General Manager Service
Textechno Herbert Stein GmbH & Co.KG
Dohrweg 65
41066 Moenchengladbach
Germany
Tel: +49 2161 6599-0
Fax: +49 2161 6599-10
http://www.textechno.com
Geschaeftsfuehrer: Dr. Ulrich Moerschel - Kommanditgesellschaft,
Sitz Moenchengladbach, Registergericht Moenchengladbach, HRA 1263
Persoenlich haftende Gesellschafterin: Stein Verwaltungs GmbH,
Sitz Moenchengladbach Registergericht Moenchengladbach, HRB 374
--------------------------------------------------------------------
Product news:
COVAFIL+: Capacitive evenness tester for filament yarns
ITEMAT+: High-speed Interlace tester with interlace stability test
FIBROTEST with extended fibre length measuring range up to 190 mm
Textechno DRAPETEST wins JEC Innovation Award
http://www.textechno.com/drapetest_award
Please visit us at the following exhibitions / events:
http://www.textechno.com/exhibitions
--------------------------------------------------------------------