Other Parts Discussed in Thread: TLV320AIC3104
Hello,
I have one problem to get the TLV320AIC3104 Control Interface functional.
On my PC WIN7 SP1 is installed.
I followed the Trouble-Shooting Guide to get the EVAL-Board to work.
1) I all Jumpers are mounted on default position
2) D2 shows Firmware Loaded
3) D7 / D5/D4 /D3 are on
4) D6 is off
5) Driver is installed and there are no Errors shown in the Decice Manager
but: => NiViUsb.sys not found ( Has XP und WIN7 the same Filename?)
=> USB-MODEVM_WDM is located in the correct folder
6) lates Version of Labview Control Panal is installed
7) USB-MODEVM ist dispayed in the device Manager
==> when I am starting the Control Panal to perform codec settings a window is popping up with the following content: "COnnect USB" ; 2 Buttons Retry and Exit
When someone could help me with this issue
that would realy help