This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3116D2 temperature is about 60C degree without audio signal input and BTL output open

Other Parts Discussed in Thread: TPA3116D2

Hi,

We have a 5.1 channel application, we use 4 pcs TPA3116D2, 

Q1: how to set the master and slave on the 4 parts.

Q2: we now set the bass channel as slave and set other 5 channel as master, the bass channel TPA3116 conected

       to one master TPA3116, other 2 TPA3116 is independent. The problem is the temperature of four TPA3116

       is higher, about 60C degree even no audio signal input and BLT output through LC filter open.

     We think the temperatur is too high. we can not position the root cause.

    Can you help on this?