Looking at the TAS5760M datasheet, I see that you show wiring the amp in PBTL mode two different ways. In figure 51, the output pins at tied before the output filter network, and in Figure 55, the PBTL lines are tied after the filter network. Is one scheme preferred over the other?
Also, there is an error in the datasheet. Figure 54 is listed as a Mono PBTL mode, but the speaker wiring is clearly stereo BTL.