I am working on a design using the PCM4222 analog to digital converter.
I have the PCM4222EVM, and I have noticed that the PCM4222 gets pretty hot. I can see that there are thermal vias on the evaluation module to help dissipate this heat. I did not see this as a suggestion in the PCM4222 datasheet. Are thermal vias like this recommended in all PCM4222 designs?
I have measured some of the voltages around the PCM4222 on the evaluation module. The voltage on VCC1 and VCC2 (Pins 4 and 9) is about 4.02V. The voltage on VREFL and VREFR (Pins 15 and 46) is about 3.78V with a master clock present, and about 3.4V without a master clock present. I know that the VREFL and VREFR pins are not to be used for external circuitry, but I just want to make sure that everything is working properly internally on the PCM4222.
I am also looking for a recommendation for a good input buffer/filter. I have read some posts that the OPA1632 that is recommended in the datasheet and used on the evaluation module is a very power hungry device. The input to the buffer/filter section of my circuit is a 2Vpp (+/- 1V) single ended signal. I am looking for a high quality Op Amp that will allow me to take full advantage of the dynamic performance that the PCM4222 is capable of. I am willing to sacrifice power and cost for performance, so if a device like the OPA1632 is the best option, then I can work with it. I am just wondering if there might be other or better options for the signal levels that I am working with.
Information on any of these questions would be appreciated.
Thanks