This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 557
Hi,
I'm working on application to amplify the signal on a 2-wire JFET based EMC. The application intend to allocate the preamp close to the EMC instead of placing on the processing board to avoid amplifying both signal and noise. Is the LMV1012 a good selection for such application, in this case parallel the LMV1012 with EMC internal JFET.
Thanks,
Kwan
Hi, Kwan,
My concern would be too much gain in your system. The LMV1012 is designed to be connected directly to mic capsules without integrated amplification.
-d2
Best regards,
Don Dapkus
Gate Driver Applications
Dallas, TX USA
We have an excellent training series that can help answer all your questions about our gate drivers. It is indexed so you can jump right to the section you want! You can find it here. A second series focused 100% on Isolated Gate drivers may be found here.
We also provide models for our gate drivers to accelerate your time to market. You can find them in the Product Folders under the "Design and development" tab:
Hello Kwan-san,
LMV1012 will be not good selection for your application because as Don-san mentioned LMV1012 connects to MIc diaphragm directly and JFET will have 0 to couple d of Gain. I'll recommend you to take LMV1032 to connect EMC with JFET. Please take look at LMV1032 dtasheet pg 9 Fig-6 which is showing how to connect with external EMC with LMV1032. LMV1032 has gain option for 6dB, 15dB and 25dB. you will select your prefered gain option.
Best regards
T NAOKAWA
In reply to Toyojiro Naokawa:
In reply to Kwan:
Your EMC has JFET interally. It means that the capacitive transducer is connenected between Gate and Source of JFET. The drain of JFET is EMC output. To work this JFET correctly, you will put RL (around 2K Ohms) via about 2V or higher.it will be depending on IDSS on JFET. LMV1012 works looks like just replacement of this JFET but has much gain. If you want to put LMV1012 close to EMC and interface to LMV1012, you still need RL and supply to give proper bias to JFET. If you take LMV1012 instead of JFET, then you can connect 2 wire at the end but need RL and supply at the end. But JFET output and LMV1012 output will be very similar which means both cases required RL and supply at the end the output is DC bias current + output current then to have voltage output, you need to put RL externally . So your EMC with JFET will be OK to use as it is. because the output style of LMV1012 is the similar to JFET. Only different is the gain. at the end point. JFET will be about 0dB or so. If you are warried about Rf noise on output line, you will put cap between output and GND at close to EMC output.