I have been trying to obtain an output from the module as delivered following the instructions in steps 2 and 3 provided. So far, with little success.
For L and R channels, I have connected both input signals (1Khz sin wave) and output resistive loads (8 ohm). 19.5V DC Power was supplied after all connections were made. Jumpers for single channel operation have been left as delivered.
I have not connected any voltage to PLIMIT. Apart from trying MUTE, I have not touched S1 or tried FAULT or made any changes to the 3 jumpers in AM AVOIDANCE. No other instructions, except a warning to only apply a voltage to PLIMIT when the power PVCC is applied, are given.
What have I missed to turn on the amplifier?