Hi:
Im designing a multichannel audio cape for BeagleBoneBlack, using the PCM3168A-Q1...
I wanted to ask if i should connect SCKI of the codec to an externall codec or if there is a pin of the mcasp0 for this function?
Can someone give me some example schematic of how clock's in the codec shoul be implemented?
I've already connected the sitara's mcasp0_aclkr (P9_42 on BBB) to the BCLKAD pin in the codec; the mcasp0_aclkx (P9_31) to the BCLKDA pin of the codec; mcasp0_fsr (P9_27) to the LRCLKAD of the codec and the mcasp0_fsx (P9_27) to the LRCLKDA of the codec. Is that OK?
mcasp0_ahclkr or the mcasp0_ahclkx can be used for SCKI?
thanks