Hello I am on the AES Standards committee 02-02 for digital audio transmission.
As a part of the review and rewrite of AES 3-4 and AES 2id, this critical question has come up.
No TI datasheets and app notes have info on this:
AES/EBU is a differential transmission on a twisted pair. It is often used in a noisy EMI environment.
1. What is the topology of the input stages of the digital audio receivers such as DIX4192, used for AES/EBU? eg differential pair? 2 hysteretic comparators?
2. What is the CMRR vs freq. of the input stages of the digital audio receivers such as DIX4192, up to VHF frequencies used in broadcast eg 100...500 MHz?
3, As digital audio PHY is RS-422 or RS-485 compatible, same question for TI interface prodicts with a differential input.
These same questions apply to ANY TI audio part with a differential digital input.
4, For TI digital audio transmitters eg DIT4192, what is the output risetime min/max into a 110 Ohm load?
Any assistance will be greatly appreciated,
With Kind Regards,
Jon D. Paul, MSEE
V.P. Scientific Conversion, Inc.