This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a board design using a TPA3118D2 amplifier. I have SDZ and FAULTZ separated. I keep SDZ low on startup and then a few seconds later I pull it high (3.3V). When SDZ is low, FAULTZ is high (5V), and it immediately swiches to low (0 V) when SDZ is switched to high.
Here is the amplifier portion of our schematic.
Any insight would be appreciated,
Dan K.
I modified our board to tie SDZ and FAULTZ together for auto-fault recovery. Before making any other changes to the board I checked the FAULTZ pin on the scope.
I then changed the caps to 1 nF and checked the scope.
The difference is significant. Still not quite there, but it looks to be an improvement.
Thanks,
Dan K.
Hi.
The scope is monitoring the FAULTZ pin. The top image is before I the changed the capacitors to 1 nF, the bottom image is after I made the change. I tried a few different capacitors in this place (2.7 nF, 100 nF, 22 pF, no cap) and saw very similar results (though I'm going from memory at this point).
Thanks,
Dan K.