Other Parts Discussed in Thread: TAS5630, TAS5630B
Hi,
we are encountering failure of the TAS5630 while taking out 230 +230W @ 4E on a 52VDC rail . The amplifier works properly till it encounters Over temperature protection ..for the first 2-3 cycles it is ok , but if we repeated the same condition the 12V rail gets shorted to gnd. And there is a weird oscillation on the output before the chip goes into protection .Kindly advise what may be the issue ,
I am attaching a link to the video we have made of the output wave form just before it goes into thermal protection .
regards
Ardhendu.