Hi,
I’m using a TPA3130D2EVM that I modified to run mono mode, I also increased the capacitors to 2*1.5mF. I’ve added an external filter with 2*100uH and 1uF. The load is a coil 1.3uH and 3.75 ohms.
I’ve tried to get enough output power using different amplification settings but I’m not able to get more than 40V swing over the load. Using a 24V power supply I would expect to get much closer to 48V. Max frequency is 500Hz so the voltage drop is only by a small part explained by the filter.
I get fairly symmetrical clipping when using sinus input.
Isn’t TPA3130D2 expected to support rail 2 rail output?
Will I get a better result using TPA3116D2 instead or does it have the same limitations?
Are there a input amplitude/amplification setting that will work?
Please advice
Martin