Hi everybody!
Thanks to the information in this forum and the PurePath Console application I have been able to get my custom hardware running quite flawlessly. However, being in the final stage of my project I encountered a problem that I haven’t been able to resolve over the past few weeks. Simply put, the configuration of the HybridFlow 4 program just doesn’t work.
I followed all the instructions provided in the “HybridFlow Processor User’s Guide (SLAU577, January 2015)” to export the register settings from the PurePath Console and I also added the required writes to exit the shutdown mode to the generated file. The initial configuration of the amplifier with the exported settings works as expected, but changes to the HybridFlow parameters have no effect on the output signal.
So although I write the same values to the amplifiers on my custom hardware as the PurePath Console does to the amplifiers on the EVM, I don’t get the same results/behavior.
First, I suspected my application on the host processor to be the cause of this problem, but after some research I found the following thread: https://e2e.ti.com/support/amplifiers/audio_amplifiers/f/6/p/432825/1550254#1550254
The reported problem is exactly the same that I am experiencing, but unfortunately there is no solution provided.
As there is little to no documentation on the HybridFlow registers I really don’t know what to try next. Therefore, I would be thankful for any help you can provide.
Regards,
Reinhard F.