Other Parts Discussed in Thread: TAS5613, TPA3100D2
I have been using the TAS5613PHD2EVM evaluation card and it has been working great in our application. I just noticed that it always operates in BD mode. And it doesn't look like I can test AD mode to see if AD mode would work better in our application.
I have already read about the differences between the modes... and understand the differences in a superficial way (what the wave forms look like and that one is more efficient than the other - as far as filtering the output. But I have some questions...
1. Is it possible to operate the TAS5613PHD2EVM evaluation card in AD mode? The switches don't look like they will let anyone do that, but what I mean is if I do some cuts and jumpers so that I can set the mode pins... would it work? Or blow up?
2. Would the output filter components need to be different?
3. Why wasn't AD mode allowed on the TAS5613PHD2EVM card? Is AD just not as useful or popular anymore? Or does AD mode have a rarely used application?
Thanks,
Bruce