This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tpa3125d2 power requirements

Prodigy 70 points

Replies: 4

Views: 252

How many Ampere it will draw ?

4 Replies

  • Hi, Michele

             TPA3125D2 is 10w/ch (SE) into an 8ohm load from 24V supply and 20w (BTL) into and 8ohm load from a 24V supply.

             The output power mentioned in above sentence are rms power.

             The over current protection trigger point is about 5.7A

  • In reply to Peter Cao:

    Thanks for your quick reply, but my question is about power supply. I know that is 24V but how many Amperes? I need this info cause I need a power supply for both TPA and preamp.

  • In reply to michele fregoni:

    It depends on your application case? How much power are you need? What is you load impedance?
  • In reply to Peter Cao:

    8ohm btl. Simple 2 stage fet preamp @ 15V for guitar use. Now I use a 24V 3A switching power supply and it's OK, but if I want to insert a reverb I need 100ma to proper operation of reverb. So I don't know if my 3A power supply (less 100ma of reverb and less 20 - 30 ma of FET preamp) are ok for TPA to operate.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.