Part Number: PCM4204
We measure the signal level of PDM using PCM4204.
Using slave mode of PCM4204, we can measure properly when the input signal to the PCM4204 DSD input terminal is up to -6dBFS PDM.
However, when we put -3dBFS or 0dBFS which is greater than -6dBFS, it overload.
Please confirm that the maximum value of PCM4204 DSD input is -6dBFS.
Also, please let us know if there is a method of testing 0dBFS in PCM4204.