This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5411-Q1: Min/Max switching frequency(400kHz/500kHz)

Part Number: TAS5411-Q1


Hi,

Could you tell me the min/max switching frequency(each 400/500kHz) for our reference?

I don't require guarantee of the value.

Best Regards,

Kuramochi

  • Hello Kuramochi-san! Brian can help you with further questions, but just to make sure we understand your question, are you looking for a switching frequency threshold? The level is set either to 400 or 500 kHz based on control register setting, and there is some nominal variablility based on many variables to include application design, temp etc, but our production test does not test absolute values but only compliance and so its difficult to give you an absolute value. Thanks, Jeff
  • Also, to give you an order of magnitude you would be looking at around +/- 5% for either 400 or 500kHz. Thanks, Jeff