Part Number: TPA3116D2
Hi,
In the process of building a system with the TPA3116D2 in a 2.1 channel set up using 8 ohm speakers. The speakers are two 3" Full Range 8 ohm drivers rated at 30W RMS (83db sensitivity) and one 6.5" Woofer 8 ohm driver rated at 50W RMS (86.5db sensitivity).
What would be the power supply requirements to get the best out of the amp and speakers. Am planning on a 24V power supply. What should be the amperage of the power supply to get the lowest THD and highest output?
Your help will be appreciated.
Regards,
Brian