Hi,
Our customer use LM4890 to drive a loudspeaker as following schematic, VDD is 3.3V from LDO which can provide 250mA current. But they encounter some problems.
1. Does LM4890 work when SHUTDOWN pin is high or low? In datasheet, it says the chip works when SHUTDOWN pin is high. However, out customer tell us the chip works when SHUTDOWN pin is low.
2. When a 3.3V level PWM signal about 8 KHz input -IN pin, the loudspeaker can make a sound, but the VDD voltage is pulled down from 3.3V to 2.2V. The loudspeaker is 400mW level, 8 ohm impedance and the drive current is about 100mA. In datasheet, we can find that when VDD is 3.3V, the output power can reach 400mW.
3. When input capacitance is added on the left of R14, and power on, the chip works after about 200ms. When input capacitance is removed, the chip works after about 100ms. And the VDD voltage are both pulled down in the two condition.
Please help to analyze these problems, thanks!