This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM4222EVM: Focusrite 18i8 not syncing properly to SPDIF

Prodigy 10 points

Replies: 1

Views: 366

Part Number: PCM4222EVM

My Focusrite 18i8 DAW interface will not sync properly to the SPDIF out of my PCM4222EVM.  My Tascam US800 will sync perfectly fine to the PCM4222EVM.  Also, when I go from the SPDIF out of the PCM4222EVM to the US800 running on another computer and direct monitoring it out through the SPDIF of that into the 18i8 and sync to SPDIF, the 18i8 syncs perfectly to it.  So, there is something about a direct SPDIF connection between the PCM4222EVM and the 18i8 that is not working right.  I have used multiple cable and power supplies for the PCM4222EVM and have no clue as to why this is happening.  Specifically, when the 18i8 is set to SPDIF sync to the PCM4222EVM, just the same way as with the US800, the sync lock light comes on but flashes randomly and of course the sound is blissful distortion and pops and everything wonderful about non-syn'c digital audio.  The 18i8 will sync to itself looping a cable SPDIF out/in.

1 Reply

  • Hi, William,

    Welcome to E2E, Thanks for your interest in our products.

    The issue you are describing seems quite strange, The EVM should work correctly with your devices. My colleague is currently taking a look to this issue and will get back to you as soon as possible.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.