Part Number: NE5532
I have an application using an NE5532 as an audio line driver (mid-rail biased, single-ended 12V supply) and have a question regarding the output current specs. Under electrical characteristics on the datasheet, the output short circuit current is listed as 38mA, which matches with the 15Ohm resistors in the block diagram of section 8.2 (600mV/15 = 40mA at current limiting). Then under Vopp, assuming 24V swing into a 600 Ohm load, I get a current amplitude of (12V/600) = 20mA, which I am assuming is a guaranteed spec. However, also listed under short circuit current is a minimum value of 10mA. In another source here on the forum I found a value for "output current" for this amplifier listed as 25mA. Does the minimum short circuit current mean that some NE5532's can only output a maximum of 10mA? I am hoping to get some clarification as to what to use as a reliable value for maximum output current for design purposes, ideally when operating from a single 12V supply.