Other Parts Discussed in Thread: TLV320DAC32, TPA6132A2, TLV320AIC26, TPA6130A2
I need to support both headphone output and line output via a single 3.5mm jack for a portable audio product. I understand the line out is a fixed 1...2Vrms output for a ~10kohm load. So I would expect the headphone output to be more than capable of supporting the line out, perhaps with lower distortion than a normal 32ohm headphone. However I am unsure as to the use of differential drivers being used for the line out application.
The product is battery powered, where they could have the USB cable attached. At which point, could there be a ground loop issue between the line out, the audio amp it's connected to and the USB connection. I have been looking to include a resistor between the audio output ground and the ground for the rest of the circuit, just to provide some isolation (10ohms).
I will perhaps have to adjust the equaliser, reducing bass to normal levels for the line out. Otherwise, I am unsure if there may be some electrical issue with implementing this approach. I will be using the TLV320DAC32 chipset in the design (waiting on EVM kit to arrive).
I have done a lot of searching, but haven't been able to find specific answers on this one.
Would greatly appreciate some expert input!