Part Number: TPA3221EVM
Other Parts Discussed in Thread: TPA3221
I have received the TPA3221EVM I ordered and it works perfectly. However, I have questions regarding the maximum PVDD allowed;
- Why is the EVM constrained to 30 VDC maximum as stated in the SLAU724B literature?
- The TPA3221 datasheet indicates that the recommended PVDD can range from 7 to 32VDC, therefore it seems the maximum recommended rail voltage can be up to 32 VDC, correct?
- I understand that the TPA3221 absolute maximum voltage is 37VDC but is not recommended for use at this rail voltage.
- Will any damage or reduction in performance to the EVM result if using up to, but not exceeding 32 VDC?
I look forward to hearing some comments.
Thanks.