Part Number: PCM1865
Other Parts Discussed in Thread: PCM1864
Hello,
I'm trying to use the PCM1865 in TDM mode, but am seeing a 6dB level difference between Channels 1/2 (the pair that is ~6dB down) vs Channels 3/4. I compared TDM vs I2S mode (using the DOUT2 on a GPIO) and the problem is only in TDM mode. Perhaps I'm missing 2 bits in TDM for the first two channels? No storage scope here at the moment to check that, but want to make sure it's not a known TDM issue. Attached images below.
I2S with 2 Serial Data Lines (looks OK):
TDM shows first channel about 6dB down: