Other Parts Discussed in Thread: OPA1622, TINA-TI, LME49600, , OPA1644, OPA1612, OPA1602
Hello dear Ti comunnity.
I've got some question regarding TIDU034 design from Ti main site.
More or less they (my questions) are related to common mode distortion and making that circuit less vulnerable?
If common mode distortion came due to impedance missmatch on IN- and IN+ then we need to make it equal on U1A stage?
We know values of input stage and let's assume that DAC output resistor will be 50-100R.
According to AD743 PDF we need to this :
Is that correct or it does not matter at all in terms of distortion in audio band?
Another question is, could we make R10 22K resistor lower? OPA160x or 164x both are very low input bias current, so I assume I can put lower resistor and it will improve noise as well, or even remove it?
How about putting same value resistor in feedback path of U1C? Circuit is using typical unity gain buffer, but it would not be diffcult to add one resistor between IN- and OUT.
Another question is about output impedance of U1D stage? Is it fixed or is it vary due to taper position of potentiometer?
This is very important because if I connect any buffer in non-inverting mode it will suffer more or less from common mode distortion am I right about this?
If output impedance is variable then should I move U1B inverting stage and buffer U1D output? Due to inverting nature of U1B my phase will be the same as input and my output buffer (which is OPA1622 as a unity gain buffer) will not suffer from common mode distortion.
Am I right all about these or maybe I should find other solution to make everything right?
If I'm right then I can make some performance upgrades with none or small additional parts which cost almost nothing - this would be nice and preffered.
I've got last question it's related to OPA1622, ATM I'm using it as a standalone buffer outside any global feedback loop.
Should I use OPA160x or OPA164x feedback loop to include OPA1622 inside it?
If yes why? If not why?
I read some documents about composite opamp stage, but it's more related to CFB opamps or opamps that are actually high input bias current/dc offset etc.
Thank you for your time, have a nice day :)