Part Number: TMDSDSK6713
Other Parts Discussed in Thread: TLV320AIC34, TMS320C6713B, PCM4204EVM, PCM1865, OMAP-L137
I would like to use TMDSDSK6713 DSK for prototype of an active acoustic noise cancelling system. TheDSK board does come with mono-mic, line-in, headphone and line-out output connectors, but I need more analog inputs.
1. Are there any daughter cards available with at least 12 audio inputs (mono)?
2. Does the board support all specified audio in/out simultaneously? In other words, can I output independent audio streams to headphones AND line-out at the same time?
3. If there are no readily available daughter cards, what would be the best interface to send the ADC outputs from a custom-built daughter card to TMDSDSK6713?
4. Would it make more sense to build a custom board with all the ADC/DACs and 6713 DSP and not use the DSK at all?
Thanks