Part Number: TLV320AIC23B
I have been using TLV320AIC32 on a breakout board (RS Components 754-1974) to record analogue signals in the range 500Hz to 5000Hz and save them as WAV files. (The board connects to a microcontroller using its I2S and I2C interface.)
I am now interested in using the same device to record analogue signals in the range 0.01Hz to 60Hz and store as WAV files. Is this possible using the TLV320AIC23B? I can't see any lower limit for frequency in the data sheet. I would sample at 8kHz.