My PCB runs fine without a HybridFlow loaded with 3 wire input.
When I try to upload a hybridflow however, it stops working.
I added this sequence to the header file as described in SLAU577A:
{ 0x00, 0x00 },
{ 0x03, 0x00 },
{ 0x2a, 0x11 },
{ 0x02, 0x00 },
{ 0x3d, 0x30 },
{ 0x3e, 0x30 },
The header file is a default Hybridflow 3 type, dumped without burst etc.
I attached the relevant piece of my code to this post.
Maybe it has something to do with a wrong external implementation of the i2c_write function?
Anybody has experience with Atmel chips in combination with the TAS575xM?