Other Parts Discussed in Thread: TAS5766M
Dear Sir,
I had finally setup the PurePath Console 1.16 on Windows 10, run it and connect it to the EVM board. Target select TAS5760XX
EVM board has power with 15V, connected 2 speaker ( 4 OHM ) at OUT A & OUT B.
After program run, it can connect the EVM board through USB. Try to play an audio on PC, it play well on PC speaker.
At AudioSwitch selection, Device 2 select Line (3-USB-AudioEVM), once this icon selected, the "ZERO" green LED will turn off. However, OUTPUT A has very tinny audio output volume,
I checked all the volume, from PC, digital and analogue are all set to maximum. Mode : Software selected.
How come the volume is so low?
I did not change any setting so far.
Am I missing something?
Thank you so much.