The PCM514x datasheet is unclear in the voltage requirements for XSMT pin.
I am using a dual supply with AVDD=3.3V and DVDD=1.8V.
8.3.3 p20: In systems where XSMT is not required, it can be directly connected to AVDD.
10.3 p63: – When the XSMT pin level reaches 2 V, soft mute process begins.
NOTE The XSMT input pin voltage range is from –0.3 V to DVDD + 0.3 V.
This information is contradictory.
Do I pull the XSMT pin to AVDD as per 8.3.3? Or to DVDD as per 10.3? If I have to pull it to AVDD, then I can't control its state with uP.
If I pull XSMT pin to DVDD=1.8V, will it be stuck in a perpetual state of mute?