I want to generate a beeping sound using the TI TLV320AIC3111. With my current codec settings, I get just a click (barely hearable from the speakers).
I am attaching a few configurations that I have already tried.
Please help me out with a script that would increase the beeping sound (Like an alarm beep.
CODEC_1.txt
0X00, 0X00, 0x41, 0x17, 0x47, 0x3F, 0x48, 0x3F, 0x49, 0x00, 0x4A, 0x00, 0x4B, 0xEE, 0x4C, 0x10, 0x4D, 0xD8, 0X4E, 0x7E, 0X4F, 0xE3, 0X50, 0XBB, 0X51, 0x80
CODEC_3.txt
Select Page 0 w 30 00 00 # PLL_CLKIN = MCLK, CODEC_CLKIN = MCLK # MCLK=2,048000Hz w 30 04 00 # DAC Instruction set PRB_P25 w 30 3C 19 # NDAC ON div=1 w 30 0B 81 # MDAC ON div=2 w 30 0C 82 # DOSR = 128 w 30 0D 00 w 30 0E 80 # DAC Volume -63.5 dB w 30 41 81 # Select Page 0 w 30 00 00 # DAC mute off w 30 40 04 # DAC power up w 30 3F 80 # Select Page 1 w 30 00 01 # Class d driver power up w 30 20 86 # Class D route enable w 30 26 95 # Class D output driver mute off w 30 2A 04 # Select Page 0 w 30 00 00 # Beep length=017700 w 30 49 01 w 30 4A 77 w 30 4B 00 # sin wave coff=23FB w 30 4C 23 w 30 4D FB # cos wave coff=7AD7 w 30 4E 7A w 30 4F D7 # Beep generate -2dB w 30 47 84
CODEC_2.txt
)
0X00, 0X00, 0x04, 0x00, 0x3C, 0x19, 0x0B, 0x81, 0x0C, 0x82, 0x0D, 0x00, 0x0E, 0x80, 0x41, 0x81, 0x00, 0x01, 0x20, 0x86, 0x26, 0x95, 0x2A, 0x04, 0x00, 0x00, 0x49, 0x01, 0x4A, 0x77, 0x4B, 0x00, 0x4C, 0x23, 0x4D, 0xF8, 0X4E, 0x7A, 0X4F, 0xD7, 0X47, 0x84,