Other Parts Discussed in Thread: TAS5760M
Dear Sirs,
My customer asked us about output voltage level of TAS5760L at THD+N≦0.8%.
When he checked on his prototype board, the output voltage was 6.8 Vrms (7.9 W).
So he was asked whether I to TAS5760L can not output of more than 8W.
I attempted to check with EVM, but there is no TAS5760LEVM.
Also he is using 32 pin type. (TAS5760MDEVM has 48 pins for EVM)
So please let me know the output voltage under the condition of THD+N≦1% with TAS5760L.
The conditions of use of the customer are as follows.
PVDD: 12 V
RL: 6 Ω
THD + N: ≦ 0.8%
Device Control: Hardware (0 dB)
Vsoft clipper: GVDD
Best Regards,
Y.Hasebe