This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3100: The time which is to turn DAC Mute ON/OFF

Part Number: TLV320AIC3100

Hi all

Would you mind if we ask TLV320AIC3100?
We would like to confirm "Figure 7-34. Example Flow For Updating DAC Digital Filter Coefficients During Play" on the datasheet P59.

Do followings mean the time which is to turn DAC Mute ON/OFF?
-DAC Volume Ramp Down WAIT Time (A)
-For fs = 32 kHz → Wait 25 ms (min)
-For fs = 48 kHz → Wait 20 ms (min)
-DAC Volume Ramp Up Time (B)
-For fs = 32 kHz → 25 ms
-For fs = 48 kHz → 20 ms


If you have some calculation formula for these, could you share us?
If you have some limitation for the time which is to turn ADC Mute ON/OFF, could you share us it?
The customer will not use filter, however they use to power down and up.
So, they would like to know it as reference.

Kind regards,
Hirotaka Matsumoto