Hi Team,
Could PCM2707C support I2S input and USB output audio ? If not, are there any other solution that could convert Analog or I2S input and USB output ?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Paul,
Got it, Thanks for your reply.
BTW, so for PCM2707C, the USB is just input, while the I2S is output, as the Figure 7 application block in spec ?
Thanks.
Hi Paul,
Thanks for your feedback.
Yes, actually customer application is converting the Analog Mic input, to USB interface output, it seems PCM2912A is exactly fit ?
Why talking about I2S input to USB output is before I find PCM2912A, and thinking adding one ADC for MIC analog input to I2S, and using one I2S to USB converter.
Could you help double confirm and suggest if PCCM2912A is most suitable solution here for TI ? And is there any AEC-Q100 device ?
Thanks for your help.
Rocson
Hi Rocson,
PCM2912A would be a very suitable part as this is one of the only USB codecs w mic bias, uPhone amp and input PGA...Since you mentioned the customer has mic input, this would be a good device with most of the functionality integrated. PCM2904 would be the only other device but it will not have mic input support as it takes line input for the ADC.
As far as Q100 qualified parts go, unfortunately none of the Audio USB converter portfolio has gone through the qualification and hence we do not have AEC-Q100 devices in this family.
Best regards,
Ravi
Hi Ravi,
Thanks for your reply here.
I have sent you Email for more details discussion on this topic, please help double check.
And I would close this ticket here then.
Thanks.