Other Parts Discussed in Thread: TPA3251
Has anyone tried a 4th-order LC filter for the output of this amplifier? (4th-order as in: inductor, capacitor, inductor, capacitor)
The switching frequency is 600kHz; a 2nd-order LC filter with cutoff frequency around 60kHz to 80kHz produces a very high output ripple. Though this is not audible, I worry that it may not play nice with the magnetic circuit of the speaker, possibly causing hysteresis distortion, leading to intermodulation distortion and other horribillities. (notice that I'm using an active crossover, so each amplifier output connects directly to an individual speaker/driver)
A quick LTSpice simulation with L1=6.8uH in series, followed by 1uF to GND, followed by 15uH in series, followed by 0.47uF to GND, with the load being 4-ohm, shows an 80kHz cutoff frequency, and approx. 80dB attenuation at 600kHz --- I will definitely sleep better knowing that there's only a few mV ripple at the audio output !!
Any comments? Any experience with trying this?
If I decide to try it, should the snubber circuit 1nF || {10nF - 3R3} be after the whole LC network, right before the speaker?
Thanks,
Carlos
--